Yes, it is possible to set the pulse output resolution of the PTO output on Lexium 32 C and Lexium 32 M. (Lexium 32 A does not incorporate PTO or PTI) The parameter defines the pulses per revolution of the PTO output of Lexium 32 is the ESIM_scale parameter.
The resolution can be freely scaled from 8 ppr to 65535 ppr. The default pulses per revolution are 4096.
When commisssioning with SoMove this parameter can be found under Parameter List > I/O functions > PTO.
The resolution can be freely scaled from 8 ppr to 65535 ppr. The default pulses per revolution are 4096.
When commisssioning with SoMove this parameter can be found under Parameter List > I/O functions > PTO.
Released for:Schneider Electric Malaysia