As more breakthroughs in technology continue to take root, the group has remained consistent in sensitizing its partners on the potential of AR, being one of the keys to digital transformation in industry. Companies must therefore capitalize on AR and pursue the opportunities that can significantly boost operational productivity and enhanced efficiency.
Speaking on this innovative technology, Belema Koleoso, Territory Technology Lead, Schneider Electric, says although much progress has been made since 2019 when Schneider Electric’s AR technology EcoStruxure Augmented Operator Advisor (EAO) was launched as a global hero offer, which works to enhance data accessibility for quicker and more accurate decision making, there remains a lethargy in the Nigerian market to adopt this technology.
Company campaigns have been run to sensitize clients to understand how EAO uses AR technology to optimize the operation and maintenance of industrial sites and equipment, AR aids effectiveness, helps to optimize human assets, and bridge the prevalent generational skill gaps. In this regard, she specifically highlighted the workforce crises that Schneider Electric foresees in the next 5-6 years, with the aged industrial population as the search for well trained workers sometimes poses a challenge.
Belema says with AR, companies do not need to lose the experience plants cultivate with the exit of a personnel, instead, years of training and experience can be “retained” through iteration of workforce turnover. For example, templates, assets, manuals can be aggregated into the EOA application, customizable by the client, it puts real-time information at your fingertips, whenever and wherever it is needed, enabling operators to superimpose current data and virtual objects onto a cabinet, machine, or plant.
This software combines contextual and local dynamic information for mobile users, enabling them to experience a fusion of the physical, real-life environment with virtual objects. It becomes a mobile work buddy for employees commencing the learning curve and in all reduces operational cost while increasing plant operational efficiency. This ensures that people who are put into the system meet the experience that others who passed through the system, left behind.
AR presents completely new ways of executing tasks, with instant diagnosis, contactless maintenance, increased efficiency, and lower cost. Industries including construction, aviation, consumer packaged goods, energy and chemical, mining and minerals etc. can use EOA to enhance their operations. The cloud-based software rides on any controller to learn activities and aggregates assets, moving past proprietary original equipment manufacturer parent protocols, to focus on the tasks.
Schneider Electric believes increased industry leaders across sectors can therefore use EOA to their advantage, where data drives processes and decisions metamorphosizing to “smart decision makers,” riding on data to make optimal decisions smarter and faster.
In retrospect, Belema says the pre-covid in Nigeria technologies like AR were seen as typical “nice to have.” She says, she highly anticipates a time when more people will understand the immense benefit of this innovation and evaluate this technology as a necessity. “Often the feedback on this is a nice-to-have, after a review of what AR offers. But I will push for people to look at it like this - When you have something that will optimize your processes, it moves from being a nice-to-have to a must have.”
To drive this renewed mindset, the AR expert opines policies such as the environmental sustainability policy, can bolster digital transformation. Stakeholders would need to advocate an optimized use of energy sustainably. Enforcement of which would naturally drive the adoption of technology across industries quicker.
“When people see that sustainability policies are enforced, for example you are penalized for not meeting a target, or incentivized for meeting a target, you would see that the case would be different. Naturally, people will begin to adopt technology to meet their goals.”
She also advocates for Nigerians to consider AR as a total cost of investment that enhances optimal output, as customers are more prone to adopt a baseline approach, where they are satisfied with running their operations minimally without incurring additional costs.
With technology improving and becoming more widely available, it is undeniable that AR would become essential for businesses to thrive in the upcoming years. Schneider is optimistic that its position as a thought leader and industry partner in the digital transformation of energy management and automation is about to gain new ground, enabling the emergence of a new landscape of energy, a paradigm shifts for the industry, and a revolutionized experience.