{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What size hole is required to mount a 9066 RA1 or 9066 RB1 OEM external reset button kit ?
Issue:
Hole dimensions for a 9066RA1 button

Product Line:
NEMA starters

Environment:
Class 9066 external reset buttons

Cause:
Determine the correct size to mount the reset button kit

Resolution:
This OEM reset kit is designed for a 30mm, 1.22" hole.

Schneider Electric Nigeria

Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.