{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
How does the CA2SKE20 alternating relay operate?
Issue:
Operation of the CA2SKE20 alternating relay's contacts.

Product Line:
Alternating Relays

Environment:
TeSys SK IEC Style Relays

Cause:
Verify if the CA2SKE20 relay will work for the customer's application.

Resolution:
The relay has 2 normally open contacts. When the alternating relay is energized only one of the contacts closes. When it de energizes this contact opens. The next time it energizes and de energizes, it alternates which contact it operates.

Schneider Electric Nigeria