undefined [object Object]
{}

Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
How can we help you today?
How can the ATV58 be run with no motor to check the output voltages?

Issue:
Wants to run the ATV58 with no motor, to check the output voltages.

Product Line:
ATV58 drives

Environment:
Run with no motor

Cause:
n/a


Resolution:
1. Confirm that the unit is at least version 4.1 IE25. (Any version earlier than this will not be able to run this test and output would be unstable.)

2. Go into menu 7 and save the existing programming to a file to be recalled when the testing is done.

3. Go to the macro-configuration menu and set unit up for material handling (Hdg).

4. Go to menu 3 (drC) Enter into the Special Motor parameter (code SPC).

Set it to PSM (Small Motor)
5. Set the OPL (output phase loss) in the FLt (fault menu) to no.

Return settings to normal when finished testing.
See the programming manual for additional details. File attached.

Schneider Electric Nigeria

Attachment(s)
ATV58 Instruction Bulletin 06-2003 VVDED397047USR603.pdf [904.84 KB]
How can the ATV58 be run with no motor to check the output voltages?

Issue:
Wants to run the ATV58 with no motor, to check the output voltages.

Product Line:
ATV58 drives

Environment:
Run with no motor

Cause:
n/a


Resolution:
1. Confirm that the unit is at least version 4.1 IE25. (Any version earlier than this will not be able to run this test and output would be unstable.)

2. Go into menu 7 and save the existing programming to a file to be recalled when the testing is done.

3. Go to the macro-configuration menu and set unit up for material handling (Hdg).

4. Go to menu 3 (drC) Enter into the Special Motor parameter (code SPC).

Set it to PSM (Small Motor)
5. Set the OPL (output phase loss) in the FLt (fault menu) to no.

Return settings to normal when finished testing.
See the programming manual for additional details. File attached.
 

Schneider Electric Nigeria

Attachment(s)
ATV58 Instruction Bulletin 06-2003 VVDED397047USR603.pdf [904.84 KB]
Explore more
Range:
Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range:
Explore more
Range:
move-arrow-top