{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What is the ATS48 line voltage operating range?
Issue:
Live voltage operating range of ATS48.

Product line:
Altistart 48, ATS48

Environment:
all

Cause:
n/a

Resolution:
The Altistart 48 is suitable for three phase supply voltages that range from 208VAC to 690VAC , 50/60Hz.  The tolerance of the voltage supply is -15% to +10%.

Schneider Electric Nigeria