{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What size fuses are used in the ATS48 for the control circuit going to CL1 and CL2?
Issue:
ATS48 fuse size for circuit control going to CL1 and CL2

Product Line:
Altistart 48, ATS48

Environment:
All open style units.  All models, All Serial numbers.

Cause:
Selection of Fuses.

Resolution:

ATS48D17Y and ATS48D22Y we recommend Class CC 600V 0.5 A fuses.

ATS48D32Y, ATS48D38Y, ATS48D47Y, ATS48D62Y, ATS48D75Y, ATS48D88Y, ATS48C11Y, ATS48C14Y, and ATS48C17Y we recommend Class CC 600V 0.6 A fuses.

ATS48C21Y, ATS48C24Y, and ATS48C32Y we recommend Class CC 600V 1.0 A fuses.

ATS48C41Y, ATS48C48Y, ATS48C59Y, ATS48C66Y, ATS48C79Y, ATS48M10Y and ATS48M12Y we recommend Class CC 600V, 1.5 A fuses.

See attached file.  Information provided in Table 31 (page 83) of document S1A37491 Altistart 48 Y-range Soft Start Controllers Instruction Bulletin.

Schneider Electric Nigeria

Attachment(s)
ATS48 Control Fuse Ratings.pdf [93.72 KB]