{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Do the NEMA 4X stainless steel enclosed combination starters include hubs?
Issue:
Hubs  from Type 4/4X (stainless steel) Sizes 0 thru 0 Enclosures.

Product Line:
Class 8538 and 8539 NEMA Contactors and Starters

Environment:
North American Products

Resolution:
Yes, combination starters in NEMA 4X stainless steel enclosures include two power cable hubs and one control cable conduit hub.

Schneider Electric Nigeria

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: