{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What are the contact ratings of 9001KA contact blocks?
Issue:
Contact ratings of 9001KA contact blocks

Product Line:
30mm Pushbutton

Environment:
9001K/SK/KX 30mm Push Buttons

Cause:
Confirm the rating of the contact block for an application.

Resolution:
The 9001 KA contacts are rated NEMA A600. The maximum AC voltage is 600VAC and the maximum thermal current is 10 amps.
9001 KA contacts are also rated NEMA Q600. The maximum DC voltage is 600VDC and the maximum thermal current is 2.5 amps.

Schneider Electric Nigeria