{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What is the nCr (nominal motor current) adjustable range on the Altivar ATV58?
Issue:
Range of nCr on the ATV58.

Product Line:
ATV58 drives

Environment:
Nominal motor current

Cause:
n/a

Resolution:
The nominal motor current parameter (nCr)  in  Drive menu 3, is from 0.25 to 1.36 of the nominal current rating for the drive (In).
In = drive controller constant torque output current rating shown on the drive controller nameplate.
The actual adjustment range is shown on the display for the nCr parameter is in terms of amps. The actual amperage range depends on the rating of the drive being used. Also, the available range is often affected by other settings such as SFt (switching frequency type) and the rEF (drive reference, HP rating) setting.
See the manual Altivar? 58 TRX Adjustable Speed Drive Controllers Keypad Display VW3A58101, bulletin number VVDED397047US.

Schneider Electric Nigeria