Search FAQs
What is the continuous current rating on the 9007C62B2 contacts?
Issue:
Checking on the continuous current rating of the contacts of a 9007C62B2.
Product Line:
9007C Limit Switches
Environment:
9007C62B2
Resolution:
See Digest 173 page 19-2. It is rated for 10 amps continuous.
Checking on the continuous current rating of the contacts of a 9007C62B2.
Product Line:
9007C Limit Switches
Environment:
9007C62B2
Resolution:
See Digest 173 page 19-2. It is rated for 10 amps continuous.
Released for:Schneider Electric Nigeria
Explore more
Range:
Explore more
Range: