Search FAQs
What is the part number for Devicenet Option on ATS48 Softstarter?
Issue:
Is Devicenet option available on ATS48 Softstarter?
Product Line:
ATS48, Altistart 48
Environment:
All
Cause:
NA
Resolution:
There is no Devicenet option card for ATS48. The built-in Communication option is Modbus.
However, part number LUFP9 Gateway is available.
The LUFP9 does require set up as it is not specific for the Altistart 48 product.
Is Devicenet option available on ATS48 Softstarter?
Product Line:
ATS48, Altistart 48
Environment:
All
Cause:
NA
Resolution:
There is no Devicenet option card for ATS48. The built-in Communication option is Modbus.
However, part number LUFP9 Gateway is available.
The LUFP9 does require set up as it is not specific for the Altistart 48 product.
Released for:Schneider Electric Nigeria
Explore more
Range:
Explore more
Range: