{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

Search FAQs

Is there a pilot light that flashes in the XB5 line?

Issue:
Flashing operation ZB5/XB5

Product Line:
Harmony XB5 22mm

Environment:
Pushbuttons

Resolution:
Part number for a pilot light with protected LED

24VAC flashing is ZB5AV18B*
110V flashing is ZB5AV18G*
* add suffix for the color of cap (1-White, 3 -Green, 4 - Red, 5-Yellow, 6-Blue).

Schneider Electric Nigeria

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: