Search FAQs
What is the part number for replacement internal red reset bar on the Class 8536 Type SF_ starter?
Issue:
Replacement Reset Bar on the Class 8536 Type SF_ starter
Product Line:
NEMA and Definite Purpose Contactors and Starters
Environment:
8536 8736 Type SF, NEMA Contactors and Starter, Size 4
Resolution:
Replacement part number for the internal, red reset bar is 31075-008-01. This piece snaps onto the overload reset mechanism.
Replacement Reset Bar on the Class 8536 Type SF_ starter
Product Line:
NEMA and Definite Purpose Contactors and Starters
Environment:
8536 8736 Type SF, NEMA Contactors and Starter, Size 4
Resolution:
Replacement part number for the internal, red reset bar is 31075-008-01. This piece snaps onto the overload reset mechanism.
Released for:Schneider Electric Nigeria
Explore more
Range:
Explore more
Range: