Issue:
GS1 auxiliary contact
Product Line:
UL 98 IEC Style Disconnect Switches
Environment:
LK4 Nonfusible and GS2 Fusible Disconnect Switches
Resolution:
Up to four auxiliary contacts can be mounted to the top of the standard switch. The GS1AD10 contact holder is only required for mounting more than the four standard auxiliary contacts. Listed below are the options for contacts which can be installed in the GS1AD10 holder.
GS1AM110 = 1 N.O. Contact Block (two can be piggy backed together - N.O. or N.C. can be mixed)
GS1AM101 = 1 N.C. Contact Block (two can be piggy backed together - N.O. or N.C. can be mixed)
GS1 auxiliary contact
Product Line:
UL 98 IEC Style Disconnect Switches
Environment:
LK4 Nonfusible and GS2 Fusible Disconnect Switches
Resolution:
Up to four auxiliary contacts can be mounted to the top of the standard switch. The GS1AD10 contact holder is only required for mounting more than the four standard auxiliary contacts. Listed below are the options for contacts which can be installed in the GS1AD10 holder.
GS1AM110 = 1 N.O. Contact Block (two can be piggy backed together - N.O. or N.C. can be mixed)
GS1AM101 = 1 N.C. Contact Block (two can be piggy backed together - N.O. or N.C. can be mixed)
Released for:Schneider Electric Nigeria