{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What class overload protection does the ATV312 or ATV320 AC Drive provide?
Issue:
What class overload protection does the ATV31 drive provide?

Product Line:
Altivar 31 ATV31

Environment:
N/A

Resolution:
Motor overload protection is based on correct adjustment of the Ith parameter in the SEt menu. It should normally be set to the value of the nameplate motor amps (FLA, Full Load Amps, FLC, Full Load Current).

Based on this setting the drive provides Class 10 overload protection.

Schneider Electric Nigeria