{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What is the bulletin number for the startup and receiving manual for the Altivar ATV66 drive?
Issue:
Looking for the bulletin number for the startup and receiving manual for the Altivar ATV66 drive?

Product Line:
Altivar Machines, Altivar 66

Environment:
All models

Cause:
N/A

Resolution:
The bulletin number is VD0C06S304 "Constant and Variable Torque: 1 to 400 hp, 460 V and 1 to 50 hp, 230 V Receiving, Installation and Start-Up".Start-Up Bulletin: https://www.se.com/us/en/download/document/VD0C06S304/Repair Parts Addendum: https://www.se.com/us/en/download/document/30072-450-73/

Schneider Electric Nigeria

Attachment(s)
Altivar-66-ATV66-User-Installation-Manual.pdf [1.34 MB]
Explore more
Category:
Articles that might be helpful Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Category: