{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What parts are needed for remote mounting the ATV61/71 VW3A1101 keypad?
Issue:
Part number required for remote mounting the ATV61/71 with the VW3A1101 keypad.

Product Line:
VW3A1101 keypad for ATV61 ATV71 drives

Environment:
All

Cause:
Installation

Resolution:

The mounting kit, including bezel and hardware is VW3A1102

The Modbus cables to connect the keypad to the control basket of the drive are:
1 Meter -      VW3A1104R10
3 Meters -    VW3A1104R30
5 Meters -    VW3A1104R50
10 Meters -  VW3A1104R100
Cable

The clear plastic door (IP 65 rating) to cover the keypad when not in use is VW3A1103

Installation Image






Schneider Electric Nigeria