undefined undefined
{}

Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
How can we help you today?
What is the heat dissipation of the Altivar 61 Drive when it is in Ready state.

The heat dissipation value of the Altivar 61 Drives when in Ready State (RDY - Drive is powered up but motor is not running) depends on the size of the Drive and of the hardware configuration that is the option cards used (like encoder card, IO extension card, controller inside card etc). 

Considering 2 option cards (2 * 3.25W) and 1 encoder card (4.25W) the heat dissipation is approximately between 34W and 53 W up to 18.5KW Altivar 61 Drives.
 
Maximum is 100W for the biggest size of Altivar 61 Drive.

Schneider Electric Nigeria

Explore more
Range:
Your browser is out of date and has known security issues.

It also may not display all features of this website or other websites.

Please upgrade your browser to access all of the features of this website.

Latest version for Google Chrome, Mozilla Firefox or Microsoft Edgeis recommended for optimal functionality.