Search FAQs
What does the 5 indicate before the coil voltage code on the LC1K****5** or LP1K****5** contactors?
Issue:
Does the number 5 on Tesys K contactors refer to the type of termination?
Product Line:
Contactors and Starters-IEC
Environment:
Tesys K Miniature IEC Contactors and Overload Relays
Resolution:
The suffix 5 indicates solder pin terminal connections instead of the standard screw clamp.
Does the number 5 on Tesys K contactors refer to the type of termination?
Product Line:
Contactors and Starters-IEC
Environment:
Tesys K Miniature IEC Contactors and Overload Relays
Resolution:
The suffix 5 indicates solder pin terminal connections instead of the standard screw clamp.
Released for:Schneider Electric Nigeria
Explore more
Range:
Explore more
Range: