{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

Search FAQs

Is there a limitation on the length of load conductor that can be used with AFI ,CAFI, and Dual Function breakers?

Issue:
Length of cable run for AFI, CAFI, or DF circuit breakers.

Product Line:
Advanced Function Circuit Breakers

Cause:
Excess cable length may interfere with circuit breaker operation.

Resolution:
The maximum length of branch circuit wiring should be no more than 250ft.

Schneider Electric Nigeria