{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What is the part number for the 24V LED pilot light used in ATV61/ 71 drives in Model 6 MCC`s?
Issue:
Which 24V LED pilot light part numbers were used for ATV61/71 drives in Model 6 MCCs.

Product Line:
ATV61/ATV71

Environment:
All

Cause:
ATV61/ATV71  LED Pilot Lights in Model 6 MCC

Resolution:
​Part number, 25501-00001 - White LED

​Part number, 25501-00002 - Blue LED
​Part number, 25501-03043 - Red LED
​Part number, 25501-03044 - Green LED
​Part number, 25501-03045 - Amber LED

Schneider Electric Nigeria