Search FAQs
What is the part number for the disconnect handle used on E-Flex Enclosed drives?
Issue:
Cusomer wants to replace a broken or inoperative handle.
Product Line:
E-Flex Enclosed Drives
Environment:
Type 1 and Type 12 - all models and part numbers
Cause:
Disconnect handle part number is not listed in the E-Flex Manual
Resolution:
The part number for the Rotary Disconnect Handle is S29338
CTA-ID : 2051053
Cusomer wants to replace a broken or inoperative handle.
Product Line:
E-Flex Enclosed Drives
Environment:
Type 1 and Type 12 - all models and part numbers
Cause:
Disconnect handle part number is not listed in the E-Flex Manual
Resolution:
The part number for the Rotary Disconnect Handle is S29338
CTA-ID : 2051053
Released for:Schneider Electric Nigeria
Explore more
Range:
Explore more
Range: