{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Can the ATV61 or ATV71 keypad be used in direct sunlight with remote mount kit VW3A1102 or VW3A1103?
Issue:
Can the ATV61 or ATV71 keypad be used in direct sunlight with remote mount kit VW3A1102 or VW3A1103?

Product Line:
ATV61 ATV71

Environment:
All

Cause:
Remote keypad in direct sunlight

Resolution:
No. The display cover is not UV protected. The display will not function properly if exposed to direct sunlight over time.

Schneider Electric Nigeria