Search FAQs
What are the NEMA and UL hazardous duty ratings on the 9007CR limit switches?
Issue:
Are the 9007CR listed for Division 2 Class I application?
Product Line:
Limit Switches
Environment:
9007C Limit Switches
Resolution:
These are UL listed for Division 1, Class 1, Groups B, C and D, and Class 2, Groups E, F and G.
Are the 9007CR listed for Division 2 Class I application?
Product Line:
Limit Switches
Environment:
9007C Limit Switches
Resolution:
These are UL listed for Division 1, Class 1, Groups B, C and D, and Class 2, Groups E, F and G.
Released for:Schneider Electric Nigeria
Explore more
Range:
Explore more
Range: