{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

Search FAQs

For ATV61/71 Ethernet IP (VW3A3316), what is the web page default password?

Issue:
How can I find the default password used to access the ATV61/ATV71 web page when using Ethernet IP Communications?

Product Line:
Altivar Drives

Environment:
Altivar 61, Altivar 71, Altivar 61Q, Altivar 71Q

Cause:
Communication card, Password

Resolution:
There are two passwords.

To get into Monitor and Setup Security:
User Name: USER
Password: USER

To get into Administrator:
User Name: ADMIN
Password: ADMIN
*This is Case Sensitive, All CAPS

Schneider Electric Nigeria

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: