{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What is the replacement for a 9001TB contact block?
Issue:
Replacement part number for a 9001TB contact block

Product Line:
Push Buttons and Operator Interface

Environment:
9001K Push Button

Resolution:
Replace with a 9001TAD1 liner and (2) 9001KA1 contact blocks.
Note that the 9001TAD1 is obsolete. The entire operator will need to be crossed to the 9001K line of pushbuttons.

Schneider Electric Nigeria