Issue:
Clarify the 22mm operator IP rating
Product Line:
Push Buttons and Operator Interface
Environment:
Harmony XB4/XB5 22mm push button
Cause:
Product Specification
Resolution:
As of 2017, all of the XB4 and XB5 push buttons are rated IP66, IP67, IP69, and IP69K or UL Type 4X.
Clarify the 22mm operator IP rating
Product Line:
Push Buttons and Operator Interface
Environment:
Harmony XB4/XB5 22mm push button
Cause:
Product Specification
Resolution:
As of 2017, all of the XB4 and XB5 push buttons are rated IP66, IP67, IP69, and IP69K or UL Type 4X.
Released for:Schneider Electric Nigeria