{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What are the supported SNMP OIDs for APC products? Where can I download the APC SNMP MIB?

Article available in these languages: Spanish

Issue
  • What are the supported SNMP OIDs for APC products?
  • Where can I download the APC SNMP MIB?
Product Line
Simple Network Management Protocol (SNMP) Enabled APC Products excluding most NetBotz products (except NetBotz 200/250).

Environment
  • All serial numbers
  • All firmware versions
Cause
For SNMP connectivity and Object Identifiers (OIDs), the APC PowerNet MIB file is required. Please see below.

Resolution
The APC PowerNet reference guide for all supported products can be downloaded from the main APC website, by searching for "Powernet", or looking for SKU "SFPMIB"

The PowerNet MIB supports all APC network-enabled devices except Netbotz. NetBotz has a dedicated SNMP MIB (excluding NetBotz 200/250).

Please note that as of v5.1.7 and higher, the sumx and sy applications also have support for the RFC1628 Generic UPS MIB. Please refer to RFC1628 MIB Compatibility with UPS Network Management Card 2 (AP9630/AP9631/AP9635) for additional information and recommendations regarding SNMP MIB use.

Schneider Electric Nigeria