{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
How To: Device Control Policy Configuration with AP9631 and AP9810

Issue

Assistance is needed in configuring Network Management Card 2 control policy (dry contact & relay I/O) configuration or verifying steps were followed properly.


Product Line
  • UPS Network Management Card 2
    • AP9631/AP9631CH
Environment
  • All serial numbers
  • Firmware versions v5.X.X, v6.X.X


Cause

For an AP9631 Network Management Card with up to two connected APC Dry Contact I/O Accessories (AP9810), you can configure its outputs to respond to events, and you can configure the UPS and outputs to respond to input alarms. Instructions are provided to assist in configuration.


Resolution

Follow the steps below in order to configure or verify an existing configuration.

Please note: The AP9810 is only supported on APP firmware 5.0.3 or higher. Even so, please make sure your APP version is 5.1.5 or higher before continuing to ensure proper on all current UPS/device models operation.


--> To begin with v5.1.X, you will want to check under the Environment Tab and set the Input Contacts and Output Relays to the desired normal state and set their severity, if applicable. Make sure you enable the input contact you wish to use or else the configuration will not be active.

--> To begin with v6.X.X, you will want to check under Configuration->Universal I/O->Input Contacts and Output Relays to the desired normal state and set their severity, if applicable. Make sure you enable the input contact you wish to use or else the configuration will not be active.


Configuring an output to respond to an event (v5.1.X)

1.) Select the UPS tab, Control Policy in the top menu bar, and by event under Event Actions on the left navigation menu.

2.) Click a category name to view all of the events in the category, or click a sub-category name to view the events in that sub-category.


3.) In the list of events, review the marked columns to see whether the required event is already configured to change the state of the output relay.

4.) To change the current configuration, click the event name, select the output relay that will change state when this event is detected, and click Apply.
Note: Control Policy configuration for output relay actions are currently unsupported for events that do not have a clearing event. For additional details, please review knowledge base article ID FA235716.



Configuring an output to respond to an event (v6.X.X)

1.) Select the Configuration menu->Universal I/O->Control Policy.

2.) Select Add Policy.

3.) Click a category name to view all of the events in the category, or click a sub-category name to view the events in that sub-category.

4.) In the list of events, review the marked columns to see whether the required event is already configured to change the state of the output relay.

5.) To change the current configuration, click the event name, select the output relay that will change state when this event is detected, and click Save Policy.
Note: Control Policy configuration for output relay actions are currently unsupported for events that do not have a clearing event. For additional details, please review knowledge base article ID FA235716.


Configuring the UPS or output to respond to an input alarm (v5.1.X)

1.) Select the UPS tab, Control Policy in the top menu bar, and by event under Event Actions on the left navigation menu.

2.) Click I/O Contact, then click the name of the event to configure.

Note: Select "Environment: A [critical|warning] fault exists for integrated Environmental Monitor input contact ({NAME.EN_US} at {LOCATION.EN_US})" for use with the AP9810 dongle. Select Environment: A [critical|warning] fault exists for external Environmental Monitor input contact ({NAME.EN_US} at {LOCATION.EN_US}) only if you are integrating with an external AP9612TH smart slot card. In APP firmware 5.1.7 and higher, the external contact options will only appear if the AP9612TH is detected.

3.) The Management Card supports up to four inputs. You must specify the input that will be associated with this event.
a.) In the Port drop-down list, select the Universal Sensor Port number (1 or 2) to which the Dry Contact I/O Accessory is installed.
b.) In the Zone drop-down list, select the zone letter (A or B) of the contact to which the input is installed.

4.) Define the action the UPS will perform when the input changes state, and select the output that will change state when this event is detected.

5.) Review your changes then click Apply.



Configuring the UPS or output to respond to an input alarm (v6.X.X)

1.) Select the Configuration menu->Universal I/O->Control Policy.

2.) Select Add Policy.

3.) Click I/O Contact, then click the name of the event to configure.

Note: Select "Environment: A [critical|warning] fault exists for integrated Environmental Monitor input contact ({NAME.EN_US} at {LOCATION.EN_US})" for use with the AP9810 dongle. Select Environment: A [critical|warning] fault exists for external Environmental Monitor input contact ({NAME.EN_US} at {LOCATION.EN_US}) only if you are integrating with an external AP9612TH smart slot card. In APP firmware 5.1.7 and higher, the external contact options will only appear if the AP9612TH is detected.

4.) Define the action the UPS will perform when the input changes state, and select the output that will change state when this event is detected.

5.) Review your changes and then click Save Policy.



Note 1: The action you configure occurs once. If you restore the input to its normal state before the alarm condition clears, the output will not change state unless the alarm condition clears and then reoccurs.

Note 2: Refer to knowledge base FA156175 for information relating to the output relay not functioning on AOS 5.1.3 and APP 5.1.3.

Note 3: Any Device Control Policy can also be reviewed via the web user interface on specified menus as well as in the config.ini file under the [DeviceControlPolicy] section.

Schneider Electric Nigeria

Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.