{}

Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
How can we help you today?
Site issues with Earth leakage
Issue:
Site issues with Earth leakage and RCD's tripping

Product Line:
Smart-UPS

Environment:
All models, All Serial Numbers

Cause:
One of the most common site issues with UPS systems is the tripping of the earth leakage circuit breakers ELCB / RCD. To examine this in greater detail, we need to look at this device: The most common RCD has a tripping current of 30mA but they are also available in other versions form 10mA - 1,000mA (1A). Selective versions, with a delayed reaction time are also available

Resolution:
The attached document looks at this issue in greater detail.

Schneider Electric Nigeria

Attachment(s)
RCD Issues.doc [57.5 KB]
Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: