{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

Search FAQs

InRow Firmware Upgrade via multiple NMC Cards(ACRC, ACRP , ACSC, ACRD)

Issue:
InRow Gen1 Firmware Upgrade via multiple NMC Cards(ACRC, ACRP , ACSC, ACRD)

Product line:
InRow Cooling

Environment:
Data Center Cooling

Cause:

Resolution:
See the attached document, which will explain how to install and execute an NMC firmware upgrade for multiple units that are using the same firmware. For example, if you have 102 ACRC101, or a total of 50 ACRP100s and ACRD500s. See list of units below that use the same firmware.

ACRC
ACRC100, ACRC101, ACRC103

ACSC
ACSC100, ACSC101

ACRD
ACRD100, ACRD101, ACRD200, ACRD201

ACRP (600mm units)
ACRP100, ACRP101, ACRP102, ACRP500, ACRP501, ACRP502, ACRC500, ACRC501, ACRC502, ACRD500, ACRD501, ACRD502


Schneider Electric Nigeria

Attachment(s)

K-B To upgrade multiple Network Management Cards ACXX series units.pdfK-B To upgrade multiple Network Management Cards ACXX series units.pdf [238.87 KB]