Issue:
Disconnecting and Reconnecting a Configured RS232-Based Sensor or Output Control Device Can Cause Device Settings to be Lost
Product Line:
NetBotz
Environment:
NetBotz 450, 455, 550, and 570.
RS232 sensor connections
Cause:
Settings associated with RS232-based sensors or output control devices may not be preserved if the device is disconnected and then reconnected.
Resolution:
Once you have connected and configured settings for an RS232-based sensor or device, do not disconnect or relocate this device unless you are prepared to reconfigure the device.
Disconnecting and Reconnecting a Configured RS232-Based Sensor or Output Control Device Can Cause Device Settings to be Lost
Product Line:
NetBotz
Environment:
NetBotz 450, 455, 550, and 570.
RS232 sensor connections
Cause:
Settings associated with RS232-based sensors or output control devices may not be preserved if the device is disconnected and then reconnected.
Resolution:
Once you have connected and configured settings for an RS232-based sensor or device, do not disconnect or relocate this device unless you are prepared to reconfigure the device.
Released for:Schneider Electric Nigeria