{}

Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
How can we help you today?
New SeaLevel PIO-48 does not work with NetBotz appliances.
Issue:

Sealevel® SeaLINK PIO-48 Part number 8203-FX is not compatible with NetBotz Appliances.

Product Line:

NetBotz

Environment:

Third party device connectivity.

Cause:

Due to an unavoidable change to the SeaIO software driver, the Sealevel® SeaLINK PIO-48 Digital I/O Adapter, Part number 8203-FX, is not compatible with NetBotz appliances. For more information, go to http://www.sealevel.com/support/.

Resolution:

To increase the number of I/O sensors that can be connected to your NetBotz appliance, the following USB digital I/O devices are supported: Sealevel SeaLINK PIO-48 - Part number 8203 only - (adds 48 digital I/O connections) Sealevel SeaI/O 462U (adds 96 digital I/O connections) Sealevel SeaI/O 463U (adds 96 digital I/O connections) Sealevel SeaI/O 450U (adds 16 digital I/O connections)

Schneider Electric Nigeria

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: