Search FAQs
Which keys are used with NetShelter cabinets and EcoAisle, and how customers can obtain them.
Issue:
Replacement NetShelter key or additional matching keys are needed.
Product Line:
NetShelter Cabinets, EcoAisle
Environment:
All versions and serial ranges.
Cause:
Keys may be lost, or spares may be required.
Resolution:
NetShelter Replacement Keys for SX, SV, AV, VX, WX and AR8132A Combination Lock HandlesReplacement NetShelter key or additional matching keys are needed.
Product Line:
NetShelter Cabinets, EcoAisle
Environment:
All versions and serial ranges.
Cause:
Keys may be lost, or spares may be required.
Resolution:
This document explains which keys are used for various NetShelter cabinets and how to obtain them.
NetShelter SX, SV, AV & VX:
Please use Part W870-8135 as the replacement key for NetShelter SX, AV and VX front & rear door handles and side panels. This is a single key, not a pair. It’s a sellable part. It can also be RMA’d for in-warrantee replacement. We allow customers one extra key per cabinet as in-warrantee replacement during the first year of ownership. If you need an in-warrantee replacement please call APC customer service and have the cabinet's model number and serial number available.
NetShelter WX:
AR100 and AR100 HD please use Part 840-0103 as the replacement key & door handle kit.
AR106, AR109 and AR112 please use W870-8135.
NetShelter CX:
Please use Part 0H-0292-SE as the replacement keys for all NetShelter CX door locks. This is a set of two (2) keys.
AR8132A Combination Lock Handles:
We do not currently stock a replacement key for the AR8132A combination lock handle. If you need to order a replacement key it must be ordered direct from the manufacturer, EMKA. or one of their distributors. The EMKA part number is 1108-U36-222. See below for EMKA contact information.
EcoAisle:
Key for drop out panels: W870-8135.
Key for the sliding door: 0J-870-26645.
EMKA contact information:
United States Headquarters: EMKA Inc.1961 Fulling Mill Road Middletown, PA 17057 Phone: 717-986-1111
European Headquarters: EMKA Beschlagteile GmbH & Co. KGLangenberger Str. 32D-42551 Velbert (Germany)Phone: +49 (0)2051 273-0
For specific regional contacts, please reference EMKA’s website. www.emka.com
Released for:Schneider Electric Nigeria
Explore more
Range:
Explore more
Range: