Search FAQs
APC by Schneider Electric - APC Surge Product Recall
Issue:
This recall involves APC 7 and 8 series SurgeArrest surge protectors manufactured before 2003. The model and serial numbers are located on a label on the bottom of the surge protector. The two numbers that follow the first letter or letters in the serial number sequence indicate the year of manufacture.
APC and the words Personal, Professional, Performance or Network are printed on the surge protectors.
The unit is included in the recall ONLY if the numbers are 93, 94, 95, 96, 97, 98, 99, 00, 01 or 02.
![How do I identify a recalled unit?](https://ckm-content.se.com/ckmContent/servlet/servlet.ImageServer?id=0158V00000CuOzWQAV&oid=00DA0000000abSmMAI)
APC and the words Personal, Professional, Performance or Network are printed on the surge protectors.
The unit is included in the recall ONLY if the numbers are 93, 94, 95, 96, 97, 98, 99, 00, 01 or 02.
Product Line:
APC SurgeArrest; The following model numbers are included in this recall. 7 Series model numbers | 8 Series model numbers |
NET7 | NET8 |
NET7T | NET8N |
NET7T-C | PER8T |
PER7 | PER8TR |
PER7C | PER8TR-CN |
PER7T | PER8TVR |
PER7T-CO | PER8XTV |
PER7T-U | PRF8T2 |
PER7TX137 | PRF8TT |
PER7-U | PRO8 |
PER7X148 | PRO8T2 |
PRF7 | PRO8T2C |
PRF7T | PRO8T2MP12 |
PRO7 | PRO8T2MP12B |
PRO7C | PRO8TV |
PRO7T | |
PRO7TX183 |
Resolution:
Contact Schneider Electric for Replacement
FYI, Due to low volume to the site, http://recall.apc.com is no longer available
FYI, Due to low volume to the site, http://recall.apc.com is no longer available
Please contact Schneider Electric IT Corp., toll-free at (800) 800-4272 option 6 from 8 a.m. to 5 p.m. ET Monday through Friday, to obtain a replacement unit.
Further Details: CPSC
Released for:Schneider Electric Nigeria
Explore more
Range:
Explore more
Range: