{}

Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
How can we help you today?
Configuring Microsoft Windows 7, 8, 10, & 11 Windows Server 2008, 2012, 2016, 2019, 2022 & 2025 to safely shutdown without using APC's PowerChute software.

Issue:
How to configure Microsoft Windows 7, 8,10, & 11 Windows Server 2008, 2012, 2016, 2019, 2022, & 2025 to safely shut down without using APC's PowerChute software.

Product:
APC branded UPS with Serial Connections

Environment:
Microsoft Windows 7, 8,10, & 11 Windows Server 2008, 2012, 2016, 2019, 2022, & 2025

Cause:
Informational

Solution:

Microsoft Windows 7, 8,10, & 11 Windows Server 2008, 2012, 2016, 2019, 2022, & 2025 do not have a native serial UPS shutdown. For a serial UPS, use the supported PowerChute software (PowerChute Business Edition / PowerChute Serial Shutdown. 

For any USB-connected UPS, these OS have some configuration for shutdown if you do not want to use the supported APC software options. Once a USB UPS is connected, the OS adds a configuration similar to that of a laptop with an onboard battery. Once this happens, you can set up a desktop or server's power options in the same way as a laptop.

Please review the attached PDF for instructions:

Also, if the native battery shutdown options are not displayed after uninstalling PowerChute software, please review Video: What to do if the system is missing native shutdown battery options / How to restore HID UPS device driver.

 

Schneider Electric Nigeria

Attachment(s)
How to configure Microsoft Vista, Windows 7, 8 , 10 Server 2008, 2012, 2016, 2019 Native Shutdown.pdf [1.89 MB]
Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range:
Your browser is out of date and has known security issues.

It also may not display all features of this website or other websites.

Please upgrade your browser to access all of the features of this website.

Latest version for Google Chrome, Mozilla Firefox or Microsoft Edgeis recommended for optimal functionality.