{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

Search FAQs

PowerChute Business Edition does not communicate on Redhat 5.0, 5.1, 5.2, and 5.3 with Xen virtualization software installed.

Issue:
PowerChute Business Edition does not communicate on Redhat 5.0, 5.1, 5.2, and 5.3 with Xen virtualization software installed.

Product Line:
PowerChute Business Edition

Environment:
Redhat 5.0, 5.1, 5.2, and 5.3 with Xen virtualization software installed

Cause:
Xen virtualization software installed, PCBE cannot communicate with the UPS because Xen opens the comm ports. Once open, PCBE can not use them for serial communications.

Solution:

If Xen is uninstalled or disabled, PCBE should have no issue with serial communications. Or, Prior to installing PowerChute, verify that a COM port is available. If a COM port is not available, you need to modify your Xen settings in /boot/grub/grub.conf. Refer to the Virtualization Guide for Red Hat Linux for more information on how to modify the Xen settings:
http://www.redhat.com/docs/manuals/enterprise/RHEL-5-manual/Virtualization-en-US/index.html

Schneider Electric Nigeria

Explore more
Category:
Software
Explore more
Category:
Software
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.