{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

Search FAQs

What communications cable is needed with my Smart-UPS and Easy-UPS with PowerChute Agent?


Issue:
What communications cable is needed with my Smart-UPS and Easy-UPS PowerChute Agent?

Product Line:
Smart-UPS
PowerChute Serial Shutdown (PCSS)
PowerChute Business Edition (PCBE) has been discontinued.


Environment:
SMX, SMT, SMC, SRT, SURTD*, SRC*940-0117B or 940-0273A (USB A to USB B)
940-0625A or 940-1525A (smart signaling serial)
940-0128D (simple signaling serial)
SmartConnect SMX, SMT, SMTL, SMC
And Non-SmartConnect SRTL
940-0504 (USB A to USB A)
940-0625A or 940-1525A (smart signaling serial)
940-0128D (simple signaling serial)
SUA940-0024 (smart signaling serial)
Standard USB A to USB B cable
C, SU, Other Smart-UPS940-0024 (smart signaling serial)
SRVMust use the USB or Serial cable that shipped with the UPS.
8-Port UPS Interface Expander940-0020 (basic port connection serial)

940-0024 (advanced port connection serial)
Interface Expander Card940-0020 (simple signaling serial)

See Schneider Electric FAQ000223363 for assistance with Easy-UPS SRV required USB drivers.
PowerChute does not discover Easy UPS On-Line (SRV/SRVL) during installation.

940-0504 (USB A to USB A)
USB A to USB A

940-0625 DB9 to RJ50
DB9 to RJ50

Standard USB A to USB B
USB A to USB B

940-0024 DB 9 male to DB 9 female
940-0024

Interface expander AP9624 card with cables 940-0020
AP9624 with 940-0020 cables





NOTE:
* SURTD model UPS devices and SRC2KUXI, SRC3KUXI, SRC3KUXIX709 devices must use the 940-0128D simple signaling cable.

Schneider Electric Nigeria

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: