{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Can a NetBotz HID door handle be used on the AR3200 NetShelter Colocation or NetShelter SV cabinets?
Issue:
NetBotz HID door handles will not latch when used on the NetShelter Colocation or SV cabinets.

Product Line:
NetShelter SX Colocation, NetShelter SV

Environment:
All versions and serial ranges.

Cause:
The hasp which ships with the HID door handles will not work on the NetShelter SX Colocation or NetShelter SV cabinets.

Resolution:

Replacement hasps for the NetShelter SX Colocation and SV cabinets are now included with the HID door handle. The original hasp must be removed and replaced.

Schneider Electric Nigeria