Issue:
Preset Speeds on ATV71
Product Line:
ATV71
Environment:
Preset speeds
Cause:
n/a
Resolution:
The Altivar 71 product line supports up to 16 preset speeds including the Low Speed setting.
Preset speeds can be selected under the Menu 1.7 Application Functions > Preset Speeds, submenu. Assignments available are:2 Preset Speeds (PS2)4 Preset Speeds (PS4)8 Preset Speeds (PS8)16 Preset speeds (PS16)Preset speeds can be triggered using Logic inputs or by changing bits using Communications. The Preset Speeds can be set from Menu 1.3 Settings or Menu 1.7 Application Function > Preset Speeds. See the ATV71 Programming manual for the logic chart and more details.
Preset Speeds on ATV71
Product Line:
ATV71
Environment:
Preset speeds
Cause:
n/a
Resolution:
The Altivar 71 product line supports up to 16 preset speeds including the Low Speed setting.
Preset speeds can be selected under the Menu 1.7 Application Functions > Preset Speeds, submenu. Assignments available are:2 Preset Speeds (PS2)4 Preset Speeds (PS4)8 Preset Speeds (PS8)16 Preset speeds (PS16)Preset speeds can be triggered using Logic inputs or by changing bits using Communications. The Preset Speeds can be set from Menu 1.3 Settings or Menu 1.7 Application Function > Preset Speeds. See the ATV71 Programming manual for the logic chart and more details.
Released for:Schneider Electric Nigeria
Issue:
Preset Speeds on ATV71
Product Line:
ATV71
Environment:
Preset speeds
Cause:
n/a
Resolution:
The Altivar 71 product line supports up to 16 preset speeds including the Low Speed setting.
Preset speeds can be selected under the Menu 1.7 Application Functions > Preset Speeds, submenu. Assignments available are:2 Preset Speeds (PS2)4 Preset Speeds (PS4)8 Preset Speeds (PS8)16 Preset speeds (PS16)Preset speeds can be triggered using Logic inputs or by changing bits using Communications. The Preset Speeds can be set from Menu 1.3 Settings or Menu 1.7 Application Function > Preset Speeds. See the ATV71 Programming manual for the logic chart and more details.
Preset Speeds on ATV71
Product Line:
ATV71
Environment:
Preset speeds
Cause:
n/a
Resolution:
The Altivar 71 product line supports up to 16 preset speeds including the Low Speed setting.
Preset speeds can be selected under the Menu 1.7 Application Functions > Preset Speeds, submenu. Assignments available are:2 Preset Speeds (PS2)4 Preset Speeds (PS4)8 Preset Speeds (PS8)16 Preset speeds (PS16)Preset speeds can be triggered using Logic inputs or by changing bits using Communications. The Preset Speeds can be set from Menu 1.3 Settings or Menu 1.7 Application Function > Preset Speeds. See the ATV71 Programming manual for the logic chart and more details.
Released for:Schneider Electric Nigeria