Search FAQs
What are the assignments for the output relays on an ATV212 ?
Issue:
ATV212 output relays assignments.
Product Line:
ATV212
Environment:
Output relays
Cause:
n/a
Resolution:
FLA, FLB, FLC are the terminals for a single pole, double throw (Form C) relay and the default assignment is ``inversion of fault relay``. Off = drive faulted, On = no drive fault. Parameter F132 can be used to change this relay function.
RYA, RYC are terminals for a single normally open contact (Form A) and the default setting is ``speed attained``. The relay contact closes when the hertz value assigned to F100 is reached. F100 is defaulted to 0. A common customer request is for ``drive running``. Parameter F130 can be assigned to 14 for ``drive running``.
ATV212 output relays assignments.
Product Line:
ATV212
Environment:
Output relays
Cause:
n/a
Resolution:
FLA, FLB, FLC are the terminals for a single pole, double throw (Form C) relay and the default assignment is ``inversion of fault relay``. Off = drive faulted, On = no drive fault. Parameter F132 can be used to change this relay function.
RYA, RYC are terminals for a single normally open contact (Form A) and the default setting is ``speed attained``. The relay contact closes when the hertz value assigned to F100 is reached. F100 is defaulted to 0. A common customer request is for ``drive running``. Parameter F130 can be assigned to 14 for ``drive running``.
Released for:Schneider Electric Nigeria
Explore more
Range:
Explore more
Range: