{}

Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
How can we help you today?
Can the ATV312 be programmed for a fallback speed in the event of a loss of the 4-20mA speed reference signal?
Issue:
ATV312 for a fallback speed configuration in the event of a loss of the 4-20mA speed reference signal

Product Line:
ATV31 and ATV312 drives

Environment:
All

Cause:
NA

Resolution:
Yes.  In the FLt menu, program LFL to LFF and then set LFF to the desired fall back speed in Hz.

Important note:
The fallback speed will take precedence, regardless of whether you are currently using the 4-20mA signal for speed control.

For example, if you are currently controlling speed with a potentiometer on AI1, and your 4-20mA signal drops on AI3, the drive will use the fallback speed even though you're currently not using the 4-20mA signal. Therefore, if you are not currently using the 4-20mA signal for speed control, you may want to set LFL to 'no', which will ignore 4-20mA signal loss.

Details on these parameters are found in the ATV312 Programming Manual on page 96.

manual screen shot
CTA-ID : 2061337

Schneider Electric Nigeria

Attachment(s)
ATV312_programming_manual_EN_BBV46385_04.pdf [1.84 MB]
ATV312 LFL and LFF parameters.JPG.jpg [120.32 KB]
Explore more
Range:
Your browser is out of date and has known security issues.

It also may not display all features of this website or other websites.

Please upgrade your browser to access all of the features of this website.

Latest version for Google Chrome, Mozilla Firefox or Microsoft Edgeis recommended for optimal functionality.