{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What is the part number for the cooling fan for the ATV61HD30N4?
Issue:
ATV61HD30N4 cooling fan part number.

Product Line:
ATV61

Environment:
ATV61HD30N4

Cause:
Requires a cooling fan replacement

Resolution:
VZ3V1206 is the heatsink fan kit.  The fans measure 3.62 by 3.62 inches each.  The kit contains two fans and this drive uses one fan kit per drive.  The fans are not available individually, it is only available as a kit.

Schneider Electric Nigeria

Explore more
Range:
Product:
Articles that might be helpful Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range:
Product: