{}

Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What is the part number for ATV61 and ATV71 Modbus TCP/IP (Ethernet) option card?
Issue:
ATV61 and ATV71 part number for Modbus TCP/IP option card.

Product Line:
Altivar 61 and Altivar 71 

Environment:
All part numbers, all models

Cause:
Customer could not find the part number

Resolution:
The part number of the Dual port (Daisy Chain) TCP/IP Ethernet option card is VW3A3310D.
VW3A3320 is also an option since it will support either ModBus TCP/IP or Ethernet IP.

Be sure to check the firmware version of your drive and confirm it's compatible with the option card.

 

Schneider Electric Nigeria

Explore more
Range:
Your browser is out of date and has known security issues.

It also may not display all features of this website or other websites.

Please upgrade your browser to access all of the features of this website.

Latest version for Google Chrome, Mozilla Firefox or Microsoft Edgeis recommended for optimal functionality.