{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What is the part number for the control terminal card on ATV71 or ATV61 drives?
Issue:
Control terminal card part number on ATV71/ATV61 drives.

Product Line:
Altivar ATV61 and ATV71

Environment:
All

Cause:
Needs to order a replacement control terminal card for the ATV61 and ATV71 drives?

Resolution:
The removable control terminal card for the Altivar 61 or Altivar 71 drive is VX4A1104; however, this part number is no longer available. You will have to order the replacement main control board part number based on the drives HP size. See the attached document.
You will see 4 choices for main control boards depending on the size HP drive they have.
VX4A61100Y lower HP ATV61
VX4A71100Y lower HP ATV71
or
VX4A61101Y High HP ATV61
Vx4A71101Y High HP ATV71

Schneider Electric Nigeria

Attachment(s)
30072-451-86.pdf [399.74 KB]