Search FAQs
What control voltage is needed for an ATS01N1..FT softstart?
Issue:
Does the ATS01N1..FT need control voltage for running?
Product Line:
Altistart 01
Environment:
All
Cause:
N/A
Resolution:
The ATS01..FT models accommodate several control voltage options:
110 - 230Vac can be connected to terminal CL2 and neutral to CL1/0
24Vac or 24Vdc can be connected (+) to terminal 24V and (-) to CL1/0
Does the ATS01N1..FT need control voltage for running?
Product Line:
Altistart 01
Environment:
All
Cause:
N/A
Resolution:
The ATS01..FT models accommodate several control voltage options:
110 - 230Vac can be connected to terminal CL2 and neutral to CL1/0
24Vac or 24Vdc can be connected (+) to terminal 24V and (-) to CL1/0
Released for:Schneider Electric Nigeria
Explore more
Range:
Explore more
Range: