{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Why does ESXi host shutdown fail if the DNS server is offline?
Issue:
PowerChute fails to shut down ESXi host/s when the DNS server is offline.

Product Line:
PowerChute Business Edition Agent versions 9.0.3, 9.1.1, 9.2, 9.2.1, 9.5, 10.x
PowerChute Network Shutdown versions 2.2.3, 2.2.4, 3.0, 3.0.1


Environment:
VMware Virtual Management Assistant (vMA)


Cause:
PowerChute runs a script the pulls the host name/s from vifptarget library. If the DNS server is running as virtual machine (VM) and has been shut down or the DNS server is off line the ESXi host name/s cannot be resolved causing the shut down to fail.

NOTE: PowerChute Network Shutdown version 3.1 and 4.x do not utilize vifptarget library. If running older versions of PowerChute Network Shutdown we recommend updated to the latest version.

Comparability information for PowerChute Network Shutdown can be found here.

To download the latest version of PowerChute Network Shutdown click here.


Solution:
Add the ESXi host/s to /etc/hosts file

Schneider Electric Nigeria

Explore more
Range:
Category:
Articles that might be helpful Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range:
Category: