{}

Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
How can we help you today?
How is a start command given to an ATS48?
Issue:
What terminations are required to start and stop on an Altistart 48

Product Line:
Altistart 48

Environment:
All models and serial numbers.

Cause:
N/A

Resolution:
The ATS48 can start with either 2 wire or 3 wire control.
For 2 wire control: Wire a jumper between the STOP and RUN terminals.  Close a dry contact between terminals 24V and RUN to start the unit.  Open the contact to stop the unit.
For 3 wire control: Wire the normally closed STOP contact between terminals 24V and STOP.  Wire the normally open START contact between terminals 24V and RUN.  Momentarily closing the START contact will start the unit.  Momentarily opening the STOP contact will stop the unit.

Schneider Electric Nigeria

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: