Issue:
Current Limit range for ILT on ATS22.
Product Line:
ATS22
Environment:
All models
Cause:
N/A
Resolution:
Set the motor current limit applied during the soft start.
With at maximum load, the ILT should be set to a high enough value to allow motor start. The range is 200% to 700% of parameter In, motor rated current. The maximum is limited to 350% of the ATS22 amp rating.
If the application requires more than 350% of the ATS22 rating, then the soft starter must be upsized.
Current Limit range for ILT on ATS22.
Product Line:
ATS22
Environment:
All models
Cause:
N/A
Resolution:
Set the motor current limit applied during the soft start.
With at maximum load, the ILT should be set to a high enough value to allow motor start. The range is 200% to 700% of parameter In, motor rated current. The maximum is limited to 350% of the ATS22 amp rating.
If the application requires more than 350% of the ATS22 rating, then the soft starter must be upsized.
Released for:Schneider Electric Nigeria